1/24/2011 7:33 AM | |
Posts: 26 Rating: (2) |
DEAR EXPERTS We are using following HMI panel: 6AV6 644 0AA01 2AX0-MULTIPANEL-MP377 - 12" This is working fine for past 11 months(commissioned in Feb2010) & now ALL OF SUDDEN we observe that the screen in this HMI panel are having lines on the edgeand also small black mark.But the screen navigation and all other functionalities are working fine. Our concern is does these lines & black marks on the screen have any issues.Plz. clarify the following: a) Any reason for lines & black marks on the screen b) Any steps / procedures / check to be done to avoid this We are having total 12 similar model HMI's in the plant.We would like to take actions to prevent this happening to ther HMI also. Expecting your advice at earliest - ASAP. Thanks Palani S Splitted from MP370 12" TOUCH downgrade to ProTool/Pro CS V6.0 SP3. |
Last edited by: O_Moderator at: 1/24/2011 2:21 PMnew subject after splitting |
|
1/24/2011 2:22 PM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is already published in the following thread 6AV6 644 0AA01 2AX0 MULTIPANEL MP 377 - LINES APPEARING ON SCREEN OF HMI. Best regards O_Moderator |
Follow us on