1/20/2019 1:08 PM | |
Joined: 4/28/2015 Last visit: 9/4/2023 Posts: 1 Rating: (0) |
Dear Experts Can anyone send me an exact manual for configuring SOE timestamping messages in Wincc. Our customer is requesting for 1ms timestamping. We are using the below digital input module in this project: SIPLUS S7-300 SM 321- DI 20-pole -25...+70 °C with conformal coating Conformity with EN 50155 T1 Kat 1 Kl A/B based on 6ES7321-7BH01-0AB0 . Digital input Isolated "16 DI; 24 V DC, 1x 20-pole," process interrupt, diagnostics, SUITABLE FOR ISOCHRONOUS MODE OPERATION model no 6AG1321-7BH01-2AB0 We have integrated backup between step-7 and wincc. We have configured interface module IM153-2 and DI module in the hardware configuration. We are unable to receive any message in Wincc runtime by checking ‘M’ in symbol table of step-7, even though the message was generated under AS messages of Wincc Alarm logging. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/21/2019 1:50:19 PMNew subject after splitting |
|
Follow us on