4/16/2024 11:31 AM | |
Joined: 5/30/2022 Last visit: 4/29/2024 Posts: 520 Rating: (85) |
Hi Jaapie, The function "PassCheckAreaPermission" is used when the Basic Process Control functionality has been executed in WinCC. In the Webnavigator manual: Limitations on the use of BPC are stated in the PCS7 WebOS manual: Supported "BPC" and "APC" functions Here it is stated that this function is supported but the WinCC Basic Process Control (BPC) plugin must be installed for use in webnavigator.
|
If this information really helps, you could use the Rate function. |
|
This contribution was helpful to1 thankful Users |
4/17/2024 11:51 AM | |
Joined: 8/3/2009 Last visit: 4/30/2024 Posts: 12869 Rating: (1642)
|
Hello Jaapie do you use the latest Update for WinCC V8? https://support.industry.siemens.com/cs/de/en/view/109818723 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on