10/31/2021 9:21 AM | |
Joined: 6/10/2009 Last visit: 1/4/2024 Posts: 36 Rating: (1) |
Hi, I have problem with FC44 block used for MOBY. Usually it happens that when it executes Command, Bit 7 is SET ACTIVE while READY is reset. when it finished execution of command vice versa happens. in some cases, i have seen that READY remains Low and ACTIVE remains high, until we need to forcefully execute CMD_NEXT and abort the ongoing command. when we abort the ongoing command, MOBY goes into fault. My intention here is to why on some occasion, Ready is kept low and active as high. i guess it gets into some sort of loop inside FC44 and doesn't come out. if anybody can help with newer version of FC44, which can mitigate this issues. thanks. ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 11/01/2021 14:29:43New subject after splitting |
|
Follow us on