5/8/2019 2:25 PM | |
Posts: 2 Rating: (0) |
Hello and thankyou for the reply! I am using the example project "FTP_1500_CODE_V20" (FTP Client scenario) provided here: FTP/FTPS communication with S7-1500 and CP 1543-1 After executing any of the commands (i.e. Retrieve or Store) an error status x8402 is shown: "The connection has an error status.The timeout of the connection may have been exceeded or the FTP server may have terminated the connection." (or "Connection in faulty state." as written in the sample project docimentation) The network configuration is according to the sample project. When simulating the hardware in PLCSIM Advanced v2.0 SP1, the CPU can be pinged from the FTP server but CP module cannot. The two are in the same network. Can FTP connection be only established directly with the CP module? If yes, then can a simulated CP module be exposed with the PLCSIM Virtual Ethernet Adapter? |
Last edited by: Jen_Moderator at: 05/09/2019 09:55:24Optimized link. |
|
This contribution was helpful to1 thankful Users |
Follow us on