9/7/2024 4:37 PM | |
Joined: 4/25/2023 Last visit: 9/11/2024 Posts: 2 Rating: (0) |
hello friends I want to define a date type memory inside a data block and set the S7_m_c attribute of that memory to true, but I saw an error that this attribute is not allowed for this type of data. If I want to read a date type data from hmi, how should I do this? I program with step7 and wincc. In addition, in scl, it is not possible to define the type of an input or output data from the date type, and the attribute S7_m_c makes it true, and it opens the same error. ------------------------------------------------------------------------------------------ |
Last edited by: Wit_Moderator at: 09/09/2024 08:24:36New subject after splitting |
|
9/7/2024 5:11 PM | |
Joined: 12/18/2014 Last visit: 9/17/2024 Posts: 33781 Rating: (4195) |
Please don't post twice for the same problem. You also made a own topic: S7_m_c attribute for date data type |
9/9/2024 8:41 AM | |
Joined: 8/21/2014 Last visit: 9/17/2024 Posts: 1024 Rating: (14) |
Closed cause question posted twice. The second thread with the subject S7_m_c attribute for date data type is published within the conference STEP 7 (TIA Portal) Best regards, |
My Forum is the place to personalize your profile, |
|
Follow us on