4/25/2024 2:19 PM | |
Joined: 5/6/2022 Last visit: 5/9/2024 Posts: 419 Rating: (82) |
Hi Landon1220, In this case, I would recommend that you review the following FAQ that I share below since it explains in detail the options that exist to perform an upload: On the other hand, in principle when you connect online with the PLC it usually tells you the version with which the project was loaded. Best regards! |
If this Information really helps, you could use the Rate function |
|
4/25/2024 2:21 PM | |
Joined: 9/21/2012 Last visit: 5/10/2024 Posts: 3937 Rating: (444) |
You need to upload the project with TIA15.1. You can't open a TIA18 project file with older TIA versions. |
Follow us on