4/5/2011 5:18 PM | |
Posts: 799 Rating: (43)
|
hello together, I think this is the official statement: Connectivity Pack best regards |
This contribution was helpful to1 thankful Users |
4/7/2011 6:58 PM | |
Posts: 133 Rating: (5) |
Maybe this link is usefull too: Best regards, kukukk
|
This contribution was helpful to2 thankful Users |
4/9/2011 2:59 AM | |
Posts: 291 Rating: (69) |
Hello everybody~ Well ~ just for your information... please take a look at printed Page.9 of the "Connectivity Pack V6.1" as attached. If you're talking about using local CLIENT access orremoteCLIENTaccess to "MS SQL Server/ WinCC instance" via MS OLEDB provider with WinCC's own "Command Procedure" & "Customer View" embedded in"MS SQL Server/ WinCC instance" when *** WinCC Basic has been installed/ ran in this local computer, then ~ I don't think it required to get extra licence such as buying "Connectivity Pack" or so ;D '------------------------------------------------------------------------------------------------------------------- The WinCC (itself) / or Connectivity Pack enables licensed access to online and archive data of WinCC. WinCC Client Access License (WinCC/CAL) A Client Access License is a license for remote access to the MS SQL Server database. If the computer performing the access has an installation of a WinCC Family product (WinCC Basic, Web Navigator, Dat@Monitor, etc.), no WinCC/CAL is required for this computer. WinCC/CAL required for remote access is already included in the WinCC Basic system as well as in the option packages, such as Web Navigator. A WinCC/CAL is required for each computer that does not have a WinCC product installed and which remotely accesses WinCC archive data on one or several WinCC servers, or processes same. The same applies for access using OPC HDA, OPC A&E or MS OLE DB Provider from outside systems.[/quote] '-------------------------------------------------------------------------------------------------------------------- Well ~ just for your information :D I hope my understanding is right, otherwise I'll have (would have been in) trouble with using my own VB.net & Excel VBA report system as an accessing client for past years! ha ha B.R., Komi AttachmentConnectivityPack_V6.1_ForWinCCSP3.pdf (749 Downloads) |
Last edited by: Komi at: 4/9/2011 4:13 AM |
|
Follow us on