6/2/2009 4:45 PM | |
Joined: 5/28/2008 Last visit: 12/8/2015 Posts: 901 Rating:
|
Hello F. Thomé, Evaluated data and statistics are shown in a table in a ruler window, statistics window or a statistics area window. The ruler window/statistics window/statistics area window are configured in the WinCC TrendRulerControl. Overview of the WinCC TrendRulerControl The TrendRulerControl can be connected with the following controls:
Depending on the data evaluation, there are three different types of windows for displaying values. The following window types are available:
All windows can also display additional information on the connected trends or columns. Requirements You have opened a picture with an OnlineTrendControl, OnlineTableControl or FunctionTrendControl in the Graphics Designer. |
6/3/2009 9:48 AM | |
Joined: 5/28/2008 Last visit: 12/8/2015 Posts: 901 Rating:
|
Hello F. Thomé, Evaluated data and statistics are shown in a table in a ruler window, statistics window or a statistics area window. The ruler window/statistics window/statistics area window are configured in the WinCC TrendRulerControl. Overview of the WinCC TrendRulerControl The TrendRulerControl can be connected with the following controls:
Depending on the data evaluation, there are three different types of windows for displaying values. The following window types are available:
All windows can also display additional information on the connected trends or columns. Requirements You have opened a picture with an OnlineTrendControl, OnlineTableControl or FunctionTrendControl in the Graphics Designer. |
6/3/2009 8:08 PM | |
Posts: 34 Rating:
|
It works. You saved me!!!!!! Very Tanks!!! |
6/28/2014 12:11 PM | |
Joined: 7/28/2009 Last visit: 5/10/2022 Posts: 90 Rating:
|
It really works!! Such a wonderful concept.... |
Cheers |
|
This contribution was helpful to
1 thankful Users |
9/16/2016 10:08 AM | |
Posts: 648 Rating:
|
Dear Sergiu.Moldovan, does your problem already exist? With best regards rh1990 |
Follow us on