7/24/2024 8:43 AM | |
Joined: 5/6/2022 Last visit: 9/9/2024 Posts: 440 Rating: (86) |
Hi AutoGen_2988568, On other occasions with this type of error, the problem was that the software had been installed on a domain and therefore did not have access to folders. Have you installed the software first outside the domain as an administrator and then brought it into a particular domain? First I would recommend creating a local user with administrator rights. Then if it doesn't work, I recommend uninstalling the software and the SQL Server outside the domain with administrator rights and then putting it in the domain if that is your case and login as a local user w/ Administrator privileges Best regards! |
If this Information really helps, you could use the Rate function |
|
Follow us on