9/26/2013 1:46 PM | |
Posts: 3037 Rating: (192)
|
Hello, Have a look for more information about faceplate in this link. http://support.automation.siemens.com/WW/view/en/68014632 Tweety |
9/26/2013 2:10 PM | |
Joined: 5/31/2011 Last visit: 4/24/2024 Posts: 190 Rating: (31) |
HeyBiLaH, Did you already find how to do it? I have the same problem!
|
9/27/2013 1:57 PM | |
Joined: 10/14/2009 Last visit: 5/2/2024 Posts: 28 Rating: (0) |
Thanks for your answer, but I can not find a solution. It explains: <<There are two options for creating a faceplate. • Creating a faceplate via the “pictures” editor. • Creating a faceplate via the “faceplate editor”>> but what I need is to create a faceplate from another faceplate (until now, copy-paste-rename), in order to add only, for example, a property or an event in the new faceplate.
|
To know, |
|
9/27/2013 2:01 PM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
New question splitted to copy&paste wincc comfort faceplates? Best regards O_Moderator |
Follow us on