5/28/2010 3:23 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, Look at Wincc Error 0x80080005 Perhaps would be helpful. Best regards, Hristo Mihalev |
5/28/2010 3:25 PM | |
Joined: 4/5/2006 Last visit: 4/24/2024 Posts: 917 Rating: (63) |
Hello ABD, hope this link can help you What can be the cause of the message "HResult Error" in conjunction with WinCC? best regards |
5/29/2010 1:32 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, As I assumed, both links in which is receiving "document is not available" - they are collected in one FAQ which you could see in my link into the last answer or the same into CBo' answer. Unfortunately if sugestions in this FAQ didn't help you to solve the problem, I am afraid you should reinstall OS. i don't know if only reinstall of WinCC will do the trick. Best regards, Hristo Mihalev |
Follow us on