9/17/2020 2:52 PM | |
Joined: 3/25/2008 Last visit: 4/3/2024 Posts: 240 Rating: (2) |
Thanks it's clearer to me. However, I take advantage of your courtesy to ask for one more thing. Once I have purchased the 100 PO package that you suggest,this seems to arrive on a stick, or a file. What i need to do to load it into the cpu? Is it done through ALM? Also what does loading this package mean? Should I stop the CPU? Do I need to reload the program? I ask these questions because the process is very delicate and reloading the sw is also a problem, there are a lot of setup data and losing one would be a problem. I didn't develop the software myself, and there are no longer who did it so I have to be very careful about what I do Thank you again ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 09/21/2020 14:00:29New subject after splitting |
|
9/17/2020 3:05 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
You can follow the exact steps in page 46. In short: 1. Order PO Expansion 2. Transfer the expansion pack to CPU via ALM and create PO activation file 3. Sent file to Siemens via SR 4. Transfer PO release file from Siemens to SEC of the CPU Can be done online in RUN If you need to remove/replace the SEC card for some reason, please note that you need to remove the CPU and thus deleting the user program with firmware <8.2. If the CPU is upgraded to firmware >= V8.2., the user program is not deleted (because it's stored permanently in the load memory). |
Last edited by: Oreca at: 09/17/2020 15:07:38If I could help you, you can use the RATE button. Thank you. |
|
9/21/2020 10:23 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hello fabioga66, you can find a detailed step for step instruction how you can upgrade your CPU with the CPU Expansion Pack in the application example Process automation with the SIMATIC PCS 7 CPU 410-5H controller. With regards |
Follow us on