12/14/2022 5:56 PM | |
Joined: 5/3/2021 Last visit: 12/6/2023 Posts: 16 Rating: (0) |
Hi, I have an IPC 627 using windows 10. It's connected to a IFP 1500 Basic HMI (6AV7862-2BD00-0AA0). There is a blue keyboard on the touchscreen that I can't get rid of or disable. This is not the same as the regular black keyboard that can be enabled/disabled through the windows settings. I think it's part of the physical HMI settings but there is nothing in the manual showing how to disable it. The manual only shows the Windows keyboard disable. I can resize the blue keyboard but can't move it around the screen. I've attached a picture. Page 48 in the link below has the only setup instructions for the Windows touch screen keyboard. https://cache.industry.siemens.com/dl/files/107/109767107/att_983371/v1/ifp_basic_operating_instructions_enUS_en-US.pdf Anyone dealt with this before? Thank you, Walks Attachmentkeyboard.pdf (422 Downloads) |
Last edited by: Walks09 at: 12/14/2022 22:37:17Last edited by: Walks09 at: 12/15/2022 13:46:45 |
|
Follow us on