3/14/2016 11:24 AM | |
Posts: 40 Rating:
|
Good idea, i shall do the same. Regards. |
3/14/2016 1:58 PM | |
Posts: 40 Rating:
|
Took me a couple of hours, but I finally solved my own problem. Solution in S7-GRAPH V5.3 for S7-300/400 Programming Sequential Control Systems. "When you save an FB, S7-GRAPH performs and implicit compilation of the block, that is, a syntax check on the sequencer you have created. Only error-free S7-GRAPH FBs can be saved and downloaded to the CPU. It is not possible to close an FB that contains errors. If you are unable to debug the program immediately, you can also save the S7-GRAPH FB as a source file or you can first create an S7-GRAPH FB source file instead of an S7-GRAPH FB. In contrast to the S7-GRAPH FB, you can save an S7-GRAPH source file containing errors at any time. " |
This contribution was helpful to
2 thankful Users |
Follow us on