8/15/2013 3:25 PM | |
Posts: 46 Rating: (1) |
S7 5.5 SP2 HF4 K5.5.2.4 CFC V7.0 SP1 7.0.1.0 ESD & F&G sytem using S7-412H with ET200M remote IO Interface via Simatic NET OPC Server to 3d party SCADA Ok, so I am working with CFC for a while now, I can get all the basics going but I am stuck however with a few issues that some knowledgeable people might be able to help me with. [schnippschnapp] 5) CPU system status. I placed the F_ SHUTDN block in my CFC to give status information regarding the safety program to the SCADA display. Is there a CFC block that will tell me if my CPU's are redundant, power supply failures etc? [schnippschnapp] other questions can be found in the following thread CFC F-system, standard MOS block CFC F-system, communications wiht my SCADA CFC F-system, Chart IO CFC F-system, Code versions CFC F-system, sometimes when I place CFC blocks on the screen they are assigned different number these are the main things I am running into, any help would be greatly appreciated |
Last edited by: O_Moderator at: 8/20/2013 10:12 AM |
|
Follow us on