11/7/2019 7:00 AM | |
Joined: 2/20/2014 Last visit: 8/18/2024 Posts: 396 Rating: (38) |
Hi, ------------------------------------------------------------------------------------------ AttachmentError screenshots.zip (426 Downloads) |
Last edited by: Jen_Moderator at: 11/07/2019 12:18:24New subject after splitting |
|
11/8/2019 1:48 AM | |
Joined: 2/20/2014 Last visit: 8/18/2024 Posts: 396 Rating: (38) |
Hi, Thank you for your reply but here's the reply that i have got via Support request that i had created earlier: Please follow this instruction: 1) Open TIA Portal in the project view (it is possible in TIA V15.1 or other version) 2) Choose in the project tree -> "Online access" -> your interface -> Update accessible devices -> Choose your device -> Online & Diagnostics 3) In this view you can see in the Diagnostics -> "General" the "Version of the TIA Portal project" This version has to be the same like you use in TIA Portal. When you use TIA V13, you have to check if the project on the PLC is with V13 without SP or with SP 1 or 2. If "version of the TIA Portal project" is V13 without SP, you will need to open a V13 project in compatibility mode. Therefore you can go to this entry: https://support.industry.siemens.com/cs/ww/en/view/82169157 and download the project 82169157_compatibility_mode_v13_v13sp1.zip (307.1 KB). Starting the project with V13 SP2 Update 2, you will be asked, if you want to upgrade your project. Then please press "No" and you will start the project in compatibility mode. Then you can upload your project to your TIA Portal. |
This contribution was helpful to2 thankful Users |
11/26/2021 5:12 PM | |
Joined: 11/18/2021 Last visit: 7/8/2022 Posts: 1 Rating: (0) |
Thank you very,very much. Finally It was a perfect solution for me after 8 hours of trying, at Friday afternoon. Even the CPU was the same. |
Follow us on