7/30/2018 9:15 AM | |
Posts: 80 Rating:
|
How can we deploy an application to many IOTs without doing it one by one? Is there any way to do it? |
9/12/2018 3:34 PM | |
Posts: 80 Rating:
|
SOLVED! After transfering the flow file, you have to post it with node-red API call. The steps to follow in the batch program are: 1. Connect to the IOT using plink.exe and remove the actual flow file (not sure if this is necessary, but it solves problem of flows running in background) 2. Transfer the file of the new flow to the IOT using pscp.exe. In this case I have export the new flow manually, and transfer it to /home/root/ directory in the IOT. 3. Connect to the IOT using plink.exe and deploy the flow with an API call. Here is an explanation of the API call, and here an example of the API call. 4. Connect to the IOT using plink.exe and reboot the system. In my case I am using a for loop that goes through a list of IPs and deploys the flow in several IOTs. |
This contribution was helpful to
2 thankful Users |
9/14/2018 6:18 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating:
|
Hello and thanks for the update! This is another method to deploy the same application on multiple IOTs. Kind regards! |
Follow us on