7/31/2021 12:26 AM | |
Joined: 7/8/2021 Last visit: 5/1/2024 Posts: 2 Rating: (0) |
Hello, I have a IPC677E with the software CPU1508(S7-1500), and I am using the port1 of the IPC for downloading the program and the port2 to communicate with the ET200SP. Initially I had several I/O modules on the ET200SP but all of them where unreachable. So I decided to keep it simple and just add a Server module. When I download the program and go online I have the error on the Server Module: A hardware component is or was inserted, but an error has occurred during module parameter assignment. * I made sure the name of the ET200SP is the same online and offline. * The firmware version of the Server Module or any other I/O is not displayed when I am going online. The firmware version of the Server Module matches. I am attaching several images of my configuration. Thank you so much, Luis AttachmentCaptures ET200SP.zip (259 Downloads) |
3/13/2024 6:20 PM | |
Joined: 12/11/2021 Last visit: 4/6/2024 Posts: 1 Rating: (0) |
I had the same problem. Thank you! |
Follow us on