8/27/2012 11:11 AM | |
Posts: 3 Rating: (0) |
Hi All I'm having a issue regard to MM 440 that sometime frequency of MM440 reduce to minimum Hz (5Hz) and then increase to Hz's working, therefore speed of motor reduce also. and input signal are 0~10V which suppied by output isolator card. So, I sent a file attached of trend speed of motor for more detailer Please give me someguides and hepl me to solve that issue And please let me know if you need to info more Thanks D.Tuan Attachmentimg-827160155.pdf (40 Downloads) |
Last edited by: O_Moderator at: 8/27/2012 12:01 PMnew subject after splitting from /tf/WW/en/Posts/79365#top |
|
8/27/2012 12:04 PM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Thread closed, because question is already published in the following thread MM 440 sometime reduce frequency Best regards O_Moderator |
Follow us on