6/10/2009 8:50 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, Look at Are there program examples for the Instruction Manual of the MICROMASTER PROFIBUS option module? and PROFIBUS GSD file for MICROMASTER 4 . What type S7-300 CPU will use? Hope this will helps. Best regards Hristo Mihalev |
6/10/2009 11:26 AM | |
Joined: 9/27/2006 Last visit: 6/10/2024 Posts: 12260 Rating: (2670) |
Hello naj; The following manual has a chapter on "Passive Components for RS-485 networks". There you will find description of Profibus-DP cables and connectors you will need for your interconnection. If you do not have special requirements for cable jacket or flexibility, then Standard Profibus cable is the normal choice. Any type of connector will have the same functionnalities. http://support.automation.siemens.com/WW/view/en/1971286 You can also look for Profibus Cable elsewhere, such as Belden 3079A for standard Profibus-DP. The attached illustration shows how to setup cable and connectors, and the use of the termination switch on the connectors at the endpoints of your network. The basic principle to remember is: one cabl;e [endpoint] Termination ON; 2 cables [inside the bus, between 2 nodes] Terminator OFF. Hope this helps, Daniel Chartier |
6/10/2009 12:05 PM | |
Posts: 3 Rating: (0) |
Perfectly clear . Thanks a lot for your help. |
6/13/2009 1:19 PM | |
Joined: 5/28/2008 Last visit: 6/10/2024 Posts: 4509 Rating: (837) |
Hello naj. I want to add a little bit info which may help you. Here's in this FAQ, you will found a pre-made FC for control MM4 via Profibus. Read the description of it in *.pdf format and also you can download it from the following link. MICROMASTER: Function block (FC14) to control an MM4 via Profibus-DP Regards, |
Ayman Elotaify |
|
Follow us on