8/30/2019 11:55 AM | |
Joined: 5/17/2017 Last visit: 12/20/2020 Posts: 64 Rating: (0) |
My problem that the temperature shown in the screen go to zero and came back to the real value within second. is the used power supply enough? The program work well with LOGO! 230 but not with LOGO 24RCE, I will upload the program file AttachmentE45B69F2-15CD-411D-8A85-2312F612FA94.MOV (258 Downloads) |
8/30/2019 1:53 PM | ||
Joined: 5/17/2017 Last visit: 12/20/2020 Posts: 64 Rating: (0) |
Do you have the opportunity to measure the current that is taken from the PSU? NO. but I tried another power supply with 1.6A no change Please check the connection on the attachment (Everything is plugged in the right hand side) Are the contact surfaces clean, no contact resistance? Yes
it occour when I change it from 230R to 24RCE AttachmentMoayed.zip (210 Downloads) |
|
Follow us on