6/5/2009 8:54 AM | |
Posts: 163 Rating:
|
Hello every1! AttachmentPLC CHANGER CONNECTION.zip (422 Downloads) |
6/5/2009 9:36 AM | |
Posts: 196 Rating:
|
This subjecct has been up some time the last months https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=22584322&caller=view |
6/5/2009 11:01 AM | |
Posts: 163 Rating:
|
Im confused only reading that link.Tell which case is applicable for my system configuration.I guess its case 4 Connecting an operator panel to the controller via two repeaters ,If im not wrong. Attachmentconfiguration.zip (302 Downloads) |
Last edited by: Sindhu@KEAS-CBE at: 6/5/2009 11:03 AM |
|
6/5/2009 1:48 PM | |
Posts: 178 Rating:
|
Is it possible yo use a Y-Link instead of repeaters? |
6/5/2009 3:08 PM | |
Posts: 163 Rating:
|
cant we achieve with the network switch?so the selection of CPU must be with MPI port and a seperate DP port Regards Sindhu |
6/6/2009 11:49 PM | |
Joined: 3/18/2009 Last visit: 5/6/2024 Posts: 306 Rating:
|
Hi Sindhu, The links described above tells you on how to connect a HMI panel on redundnant profibus. (repeater solution is for that) In your configuration you are connecting your MP 377 on ethernet. Your configuration looks good. You need to use the "ChangeConnection" script in WinCC Flex 2008 to switch between the CPUs. Inthis FAQ, it is described how to use this function with MPI. However the same holds true for ethernet. You just need to configure equivalent ethernet connections instead of MPI connections described in the FAQ. The other steps remain the same. The catch though is, you require WinCC flexible 2008. (Earlier versions don't support ChangeConnection for ethernet. See section 1.2, page 4 of 9 of the attachedFAQ) regards. Attachment35508221_change_connection_e.pdf (359 Downloads) |
6/8/2009 12:24 PM | |
Joined: 3/18/2009 Last visit: 5/6/2024 Posts: 306 Rating:
|
Hi Sindhu, For MPI, you will need to then connect an MPI cable between all CPUs. Considering your existing configuration and assuming that you second H-Station is on the same ethernet network, you can choose FCs AG_SEND and AG_RECV to communicate between them. See thisFAQfor details. A sample project is also installed in example folder of Step 7. (See attached pic)
|
6/8/2009 2:29 PM | |
Posts: 163 Rating:
|
Whats the diff between S7 connection, fault-tolerant,and ISO transport connection.I think s7 connections is more suitable for our project AttachmentCONNECTION.zip (246 Downloads) |
Follow us on