9/5/2010 5:40 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello Sandy Kalsi, Yes, Davesh is right. The perfect solution is to use T400... But my points are in other side. I don't know what type of SSD - Eurotherm Drives you had there. The project requirements are also very important. But: basically we could say Siemens analog is MM440. If I were in your place, I would check wire connections with encoders there and to look deeply into drive's parameters how drives communicate and do the job. Eventually foror MM440 you would need How should I set up the encoder module? plus CD manuals which are going together with each MM440. (BTW you could find them here also). Take all info from old system and contact with Siemens center. (Davesh is right also for this). P.S. Davesh, 2 times rught = 5 stars. Best regards, Hristo Mihalev |
This contribution was helpful to1 thankful Users |
6/4/2014 1:19 PM | |
Joined: 9/1/2005 Last visit: 3/5/2024 Posts: 4097 Rating: (193) |
follow upquestion published by Aniteeianis splitt to a seperate thread with the subject application in Servo V90 drive. Best regards CS_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on