2/7/2024 5:14 PM | |
Joined: 10/12/2021 Last visit: 4/18/2024 Posts: 8 Rating: (0) |
Hi Experts I had Migrated a Project from Wincc V7.0 Sp3 to Wincc V7.3 SE. The migration Completed Successfully without any error. But Now in the Migrated project C script for the Pop-up is not working. when i press the button for the pop up, the diagnostic window gives some error. Can Someone help me to resolve this issue and why this problem is coming as this project backup is already running properly in the wincc V7.0 I have attached the C script and diagnostic window. Thanks & Regards Muktdir AttachmentPOPUP_C_Script and diagnosic.txt (127 Downloads) |
Follow us on