5/17/2012 2:46 PM | |
Posts: 56 Rating: (1) |
Hi Is it possible to connect MM420 ( 6SE6420-2UC23-0CA1 ) to main voltage supply Thank u… |
5/18/2012 7:34 AM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835)
|
Hello, As IBN-Service answered in his first post, He made it Bold for you "1/3AC200-240V +10/-10% 47-63HZ". Numbers are the same in English & German. In any case, here is the link of the MM420 drive.6SE6420-2UC23-0CA1, As adviced by friends here, You can power it uising 1/3 phase 240VAC. For you case, power it using 1 phase, 240VAC, 50Hz. ##Attached connection diagram## Hope this helps.
Attachmentconnection.pdf (147 Downloads) |
Last edited by: Ayman Elotaify at: 5/18/2012 7:39 AMAyman Elotaify |
|
This contribution was helpful to1 thankful Users |
5/18/2012 7:50 AM | |
Posts: 56 Rating: (1) |
Dear Ayman Is there any risk as the the power supply ratewill beat the max limit 240 VAC ... Thank u... |
5/18/2012 9:39 AM | |
Joined: 4/21/2006 Last visit: 4/16/2024 Posts: 510 Rating: (24) |
I deleted the non-technical postings. Regards, Blue Moderator |
This contribution was helpful to2 thankful Users |
Follow us on