9/2/2022 10:12 AM | |
Joined: 10/4/2011 Last visit: 3/25/2024 Posts: 4 Rating: (1) |
Hi Everybody, I have a problem with CIP client communicating with a Contrologix PLC running V12. The comms are not robust enough for the production line it is operating on. Our panel is the first piece of Siemens on site because the customer is migrating to Siemens. The PLC is a 1214 with the code written in V16. The comms will randomly drop out which obliviously stops the whole production line. I know the network is quite busy with no IP address duplications. The drop out will definitely occur if I go to monitor mode with either PLC. I am only transmitting and receiving 6 Words. Any suggestions to make thing more reliable? Martyn Walden ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/14/2022 10:55:32New subject after splitting |
|
Follow us on