3/21/2022 4:09 PM | |
Joined: 9/27/2006 Last visit: 5/21/2024 Posts: 12257 Rating: (2668)
|
Hello tystnariluren: What exactly do you mean by "What type of communication would you recommend between these 2?" Which 2, there are 2 PLCs and one MV500 scanner in your project, no? The title of your thread implies you are looking for connections between the CPUs, S7-300 to S7-1500. If that is so, do they have a common interface, Profinet, Profibus,,, Once that is determined, it is easy to establish communciations between 2 CPUs. Also, Siemens proposes Profinet between the MV500 optical scanners and a PLC, as you can see from this product presentation and the MV500 manual: - Product Note: MV550 S and MV550H: https://support.industry.siemens.com/cs/ww/en/view/109769656 - Manual MV500: https://support.industry.siemens.com/cs/ww/en/view/109759658 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 03/21/2022 17:42:21 |
|
3/22/2022 12:16 PM | |
Joined: 8/3/2009 Last visit: 5/17/2024 Posts: 12970 Rating: (1651) |
Hello tystnariluren If you just want to communicate between Siemens 300 (simatic manager) <> 1500 (TIA17) as mentioned in the caption of your topic then have a look at: https://support.industry.siemens.com/cs/de/en/view/78028908 Chapter 21.4.5 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on