9/27/2010 12:40 PM | |
Joined: 9/28/2007 Last visit: 2/20/2024 Posts: 234 Rating: (12) |
Dear all, i am checking siemens simoreg K 6RA22 drive on bench without motor. i have connected two 200 watt bulb in series and conected on Armature output. When i enable terminal 17,18 the drive parameter P00 shows II and both bulbs on for short time and immediately display F19.in manual F19 show " no current can flow from armature". Tell me briefly where is the fault. fault is from hardware side or from parameter setting. can you help me about above fault Splitted from Simoreg k 6RA22 Reset Parameter to factory setting. |
Last edited by: O_Moderator at: 9/27/2010 12:51 PMnew subject after splitting Muhammad Munir |
|
9/27/2010 12:52 PM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is already published in the following thread Simens Simoreg K 6RA22 show F19 . Best regards O_Moderator |
Follow us on