6/4/2024 9:54 AM | |
Joined: 7/19/2022 Last visit: 6/25/2024 Posts: 371 Rating:
|
Hello AutoGen_6637653, The label that you attached indicates the following: 6ES7647-7B...-...0 is fixed for all the IPCs 427C - K: Processor: Core2 Duo 1,2 GHz, 800 MHz FSB, 3 MB SLC, Profibus DP 12 - 4: Main memory: 4 GByte, DDR3 1066, SDRAM - 0: HW extension: without HW extension - 4: Drive: 8 GB CompactFlash changeable - A: Internal drive: 80 GB HDD SATA - M: OS: Windows Embedded Standard 2009 preinstalled on mass storage changeable |
If this Information really helps, you could use the Rate function |
|
Follow us on