1/31/2018 11:02 AM | |
Joined: 1/30/2018 Last visit: 9/20/2018 Posts: 5 Rating: (1) |
Hi, Could I please ask if this would be the same for my setup. I am trying to connect a D445-2 from a Simotion Scout v4.4 project to a TIA v14 project with Comfort TP1200 HMI via device proxy. Everything is coming across OK except for the UDT data -UDT is showing under PLC tags but the list is empty. Am I right in saying the answer is the same as to the issue above, or is there any way this can be done when linking Scout to TIA project? Many thanks, Barry
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/1/2018 9:43:57 AMNew subject after splitting. Inserted quotation. |
|
Follow us on