11/11/2022 6:29 PM | |
Joined: 2/17/2020 Last visit: 5/21/2024 Posts: 1004 Rating: (175) |
Hi again, If you do not intend to program a SCADA system in TIA Portal, you can download the first software package from the following link (WinCC Basic/Comfort/Advanced) to install TIA Portal parallel to WinCC V7 without SQL database conflicts. If you intend to program a SCADA system in the TIA Portal, you should install WinCC Professional then, but you cannot install WinCC V7 afterwards for the reason already mentioned. In this case, the only alternative would be to create a virtual machine with either of the two SCADA software inside and the other one on the host. I hope this helps! |
A rating will be well appreciated. |
|
Follow us on