4/14/2018 1:46 AM | |
Joined: 12/12/2013 Last visit: 4/30/2024 Posts: 31 Rating: (1) |
I am having a similar but slightly different problem. When alarms are triggered in the CFC, the chicklet on the WInCC HMI flashes accordingly. However, no message in the alarm banner comes up. The operator from HMI can acknowledge the alarm and it clears as it should. If I delete the CFC block and add then add new one and then do a changes only compile and download to the server, it works fine. So I know how to fix, but it is painful and laborious... Is there a better way to fix this than deleting and re-adding every block in the controller???? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/16/2018 10:03:08 AMNew subject after splitting |
|
Follow us on