10/7/2013 9:31 AM | |
Posts: 150 Rating: (17) |
Dear All, I have setup a system using WinCC And Downtime Monitor. All works fine on the server. My Client asked me to install Datamonitor to the system so that 25 users of the company can monitor WinCC. Issue #1 I have set up Datamonitor and it works excellent in windows XP. In windows 7 (IE V10) I have the following issue: On the top of the Internet explorer a text appears and the webnavigator menu on the right is not accessible (see attached #1). My guess is that the menu structure is not translated correctly in HTML. Issue #2 I have setup Downtime monitor as per the installation manual chapter 4.2.2 and I succesfully installed the PI-Plugin to the webnavigator client from the download area. The problem I face is that when I login to webnavigator an error appears saying that the user has no access rights to the control (see attached #2). I gave the DataMonitor users the following rights from the WinCC user administration: DTM_READ_DATA DTM_CHANGE_CONFIGURATION DTM_MODIFY_DATA Any help will be highly appreciated. Regards Nik Attachmentattachments.zip (108 Downloads) |
Last edited by: Nikzitronik at: 10/7/2013 9:31 AM |
|
Follow us on