5/10/2021 9:39 AM | |
Joined: 10/13/2008 Last visit: 12/2/2022 Posts: 73 Rating: (4) |
Hello TechnoBlaze Thank you again for your attention. Fortunately the software was installed successfully . The problem was a dll file in SQL source program that has been missed. Now My problem is the speed in opening of WINCC. When I create a new project or open an old project the wincc project opens very slow ( about 5 minute ) My laptop is a core i7-10th Generation, 8G RAM, 128 GByte SSD and 1TB HDD. Best Regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/10/2021 14:11:58New subject after splitting |
|
5/11/2021 11:15 AM | |
Joined: 10/13/2008 Last visit: 12/2/2022 Posts: 73 Rating: (4) |
Dear Experts, Thanks to Moderator to move this topicfrom PCS 7 to WINCC conference. To illustrating the problem, I have to say that Firstly I install a new copy of PCS 7 V9.1 on my laptop. and the problem is creating Simatic Station or Opening Wincc on this system is very slow ( opening wincc explorer not runtime) Thanks to everybody that can help me to solve this problem. Best Regards. |
Last edited by: r_nakhai at: 05/11/2021 11:17:08 |
|
This contribution was helpful to1 thankful Users |
11/30/2021 2:48 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2149)
|
Hello KUMAR VINEET,
It is solved with the actual Update 6
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
This contribution was helpful to1 thankful Users |
4/16/2022 11:35 AM | |
Joined: 1/28/2010 Last visit: 5/27/2024 Posts: 66 Rating: (0) |
I also faced this problem. It is solved by installing Update7 Shankar |
Follow us on