11/8/2023 3:54 PM | |
Joined: 12/23/2021 Last visit: 2/21/2024 Posts: 234 Rating: (23) |
Hi! I didn't heard about this problem but I recommend you to upload WinCC V7.5 SP2 to the lastest update available (Upd14) from the following link: Updates for WinCC V7.5 SP2 and WinCC V7.5 SP2 ASIA Maybe it could helps. Let us know the results after install the update. |
If this post helped you in any way, please rate it positively. |
|
11/9/2023 12:32 AM | |
Joined: 9/3/2008 Last visit: 5/30/2024 Posts: 923 Rating: (158)
|
Hi, You have not described the kind of system that WinCC is running on, but the way you descritbe the behaviour could sound like you connect to the WinCC via remote desktop and after disconnect and connecting again, you don't see the picture and then try to start graphics runtime but it will not start. This is probably because it is already running under another session. Running WinCC via Remote Desktop is not supported unless it runs as service, and then only as a maintenance under certain restrictions. See this FAQ for remote access to WinCC. I hope this helps. |
Michael |
|
Follow us on