9/21/2011 8:57 AM | |
Joined: 9/8/2005 Last visit: 3/7/2024 Posts: 177 Rating: (15) |
Hello, if you are working with redunatd servers, it is strongle recommanded to use the described User Archive functions. Otherwise the redundance mechamisen isn't work. Generall yis the better solution to using the C user Archive function. I know it is much more complicate and not so fast, but the best solution. Possible that the WinCC tool "script Connector" is helpful for your task. It allows to using C-Funktions in VBS scripts. http://support.automation.siemens.com/WW/view/de/17544346 Michel |
Follow us on