11/13/2024 6:54 AM | |
Joined: 11/13/2024 Last visit: 3/18/2025 Posts: 6 Rating:
|
How can I clear data logs of historical Trend in Runtime? I am using TIA v15.1 Wincc Professinoal ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 11/13/2024 08:16:21New subject after splitting |
|
11/14/2024 11:08 AM | |
Joined: 7/19/2022 Last visit: 9/16/2025 Posts: 436 Rating:
|
Hello AutoGen_7532017, In WinCC Professional I think that you can only delete / reset the historical data in the transfer mode (Download to device/ Download to file system) in the load preview window, not in Runtime. There you have the possibility to select between retain and reset the existing historical data. Have a look in the attached screenshot and the following FAQ: |
If this Information really helps, you could use the Rate function |
|
11/14/2024 2:26 PM | |
Joined: 11/13/2024 Last visit: 3/18/2025 Posts: 6 Rating:
|
thank you but i want to delete trend diagram BCZ if one trend cycle diagram complete then second cycle diagram it overwrite in old cycle diagram that is the problem and then save pdf report so i cant define single cycle and cant delete old cycle diagram i attachment both pdf report and also attach overwrite diagram photo in my first query AttachmentD6THB-40101.12.11.24.pdf (218 Downloads) |
Follow us on