4/3/2006 2:33 PM | |
Posts: 1084 Rating: (72)
|
Just soI don't mis-understand you: Did you declare one function or multiple functions in one .bmo? with regards, Ikkezelf |
4/3/2006 6:51 PM | |
Posts: 14 Rating: (0) |
I've declared more functions in one new .bmo and I want to call them from another function (or functions)in another .bmo file. ADP |
4/12/2006 12:04 PM | |
Posts: 14 Rating: (0) |
I've tryed with the script debugger, but without success. I solve the problem by copy the function GetTag and SetTag from TagManager.bmo to INIFiles.bmo as new Private Function and Sub. In any case I include 2 bmo files one is used to read INI files from the project folder to declare constant to a data set. The function that is not working is the SetTagFromINI that call sub SetTag. Calling SetTag from SetTagFromINI return me a message "SetTag variable not defined" if I not declare SetTag as Private Sub into INIFiles.bmo!!! Bye AttachmentScriptLib.zip (559 Downloads) |
4/13/2006 4:17 PM | |
Posts: 14 Rating: (0) |
It is clear! Thanks |
Follow us on