Industry Online Support
Technical Forum
5/23/2006 2:40 AM | |
Posts: 122 Rating: (4) |
[:o]Dear experts: I am very confused about my WINCC use.The WINCC installation software is integrated in the PCS7 installation software,the installation of WINCC need SQL SERVER 2000 SP3 ,WIN2000 SP4,IE6.0SP1,and all these have been in my operation system(win2000 professional).During installation there is not any alarm or warnning,but when I open WINCC and creat a new project after the installation is fifnished there is an alarm pop up just showin the attachment.I have tried several times and also in other operation systems but no function.and my question is that do i need to update the operation system (win2000 professional)to the latest ,or may be there is a relationship with my hardware components,I am very grateful if somebody can give me some advice or guide. Attachmentwincc error.zip (624 Downloads) |
Last edited by: peters at: 5/23/2006 2:46 AM |
|
5/23/2006 7:57 AM | |
Posts: 3149 Rating: (171)
|
Hi, |
5/30/2006 3:55 AM | |
Posts: 122 Rating: (4) |
it's ok now ,thanks very much! |
Follow us on