6/3/2006 5:15 AM | |
Posts: 122 Rating: (4) |
dear experts: now i have a problem about my SFC in wincc.after i have created a project in my computer,i tested the CFC and SFC in my computer with the help of PLCSIM software,and these two are successful without errors.but when i open the SFC in wincc according the guide manual and want to run it ,the "start"button is not active ,so i compared my SFC with the one in the guide manual and found that my SFC is not ready for running(show in the title of the SFC pattern in my documents),the PLCSIM is already running,and the SFC is also OK in the simatic manager ,i don't know what's the problem is ,i need your help seriously.(there is also awincc alarm generated"the group display hierarchy is not up-to-date",i don't know if there is any relationship between these two) Attachmentdocument1.zip (583 Downloads) |
Last edited by: peters at: 6/3/2006 5:29 AMLast edited by: peters at: 6/3/2006 5:25 AMLast edited by: peters at: 6/3/2006 5:23 AMLast edited by: peters at: 6/3/2006 5:21 AMLast edited by: peters at: 6/3/2006 5:20 AMLast edited by: peters at: 6/3/2006 5:19 AM |
|
6/4/2006 6:02 AM | |
Posts: 122 Rating: (4) |
dear nemo: what is your meaning about"WINCC picture tree"?is it means that the "graphic designer"?i have already saved but no function. |
6/4/2006 7:50 AM | |
Posts: 122 Rating: (4) |
dear nemo: i have saved the "picture tree manager"according your advice.and the alarm"group display hierarchy"never come again.but the WINCC main picture is also inactive,just gray ,no colorful,operation forbidden.if we want to active the WINCC do we need to use a real CPU not a PLCSIM software? Attachmentdocument1.zip (566 Downloads) |
Last edited by: peters at: 6/4/2006 7:54 AM |
|
6/4/2006 7:52 AM | |
Posts: 122 Rating: (4) |
document2
Attachmentdocument2.zip (505 Downloads) |
6/5/2006 11:30 AM | |
Posts: 122 Rating: (4) |
dear nemo: i have checked the MPI address in hw-config,it is right.i also studied the doucuments whose web site you showed upstairs,and found that i haven't created the connection betwwen PLCSIM and WINCC,so i did this later,but the wincc is also inactive,i have made screenshot shows in the documents,and according these documents there are questions follows: 1.is it because that there is no connection between wincc and s7 so leed to failure 2.must we install programs in this squence: STEP7/CFC--PLCSIM--WINCC,if we install wincc first then plcsim can it leed tothe failure of connection between PLCSIM and WINCC? 3.the cpu slot shows in my document is 3 although this cpu take place of two slots? i would like to express my great thankness to you for your reply. Attachmentdocument.zip (566 Downloads) |
Follow us on