6/18/2024 11:37 AM | |
Joined: 1/17/2013 Last visit: 10/16/2024 Posts: 1106 Rating: (6) |
Dear Experts, I use WinCC V8.0 and I have the warning windows message as pictue when I try to open the projject filewhich made from WinCC V7.5 at another computer. The message is "Cannot open WinCC -Project Manager for configured server is not running. Check the computer name of the server" How can I sovle this problem ? Best Regards, Vorapob
AttachmentWinCC Cannot open WinCC Project Manager for configured server is not running.jpg (229 Downloads) |
Best Regards, |
|
6/18/2024 11:59 AM | |
Joined: 8/12/2021 Last visit: 10/16/2024 Posts: 325 Rating: (30) |
Hi! I know is not the same error, but to discard and in case the process was blocked, I would delete certain files such as the lck that is explained in this FAQ |
If this Information really helps, you could use the Rate function |
|
Follow us on