6/25/2012 10:00 AM | |
Posts: 49 Rating: (1) |
Dear Experts, Could you help me? My customers are using Emidate(computer have CP5613_profibus): connect to 2 ET200U stations. They want to use ET200M because ET200U cant order and buy them. They want to keep Emidate program and want to change ET200M. In Emidate program /parameters, i can choose type of modules for ET200. I changed them to S7 module. But it only digital module recieved but analog module not. Now, value of analog module get max:22,96mA and flag at 'O'. in the past(using module of ET200U), value of them under 22,96mA and flag at ' ' . What should I do. Thanks in advance
Attachment25 06 12 analog.pdf (69 Downloads) |
Last edited by: SIS AN at: 6/25/2012 10:03 AM |
|
6/25/2012 10:17 AM | |
Posts: 49 Rating: (1) |
value of analog and flag now:
Attachmentanalog now.pdf (61 Downloads) |
3/20/2013 4:08 AM | |
Posts: 49 Rating: (1) |
HiHarald Ott, Please send me the further information about Emidate v6.0. Thanks. |
Last edited by: O_Moderator at: 3/20/2013 7:31 AMcontact data deleted |
|
Follow us on