7/17/2023 8:53 AM | |
Joined: 7/19/2022 Last visit: 8/12/2024 Posts: 380 Rating:
|
Hello PolaNanElias, For use in areas with special requirements, the following variants are available panel: • Comfort PRO Panels, IP65 protection and integral Type 4X/12 for use next to the machine or in harsh environmental conditions. • Comfort Outdoor Panels for indoors and outdoors, e.g. eg oil and gas, marine or refrigeration techniques. • Comfort Panels INOX for environments with high requirements in terms of safety and hygiene, such as the food industry, the tobacco industry and the like, the pharmaceutical or fine chemical industry. How resistant to chemicals are the SIMATIC HMI operator panels and Industrial PCs? |
Last edited by: JBS98 at: 07/17/2023 08:53:24If this Information really helps, you could use the Rate function |
|
7/17/2023 11:18 AM | |
Joined: 8/25/2007 Last visit: 6/7/2024 Posts: 17 Rating:
|
Thank you for your reply So according to it we can say that I can recommend the INOX panel for that application?
|
7/27/2023 12:33 PM | |
Joined: 8/3/2009 Last visit: 8/15/2024 Posts: 13561 Rating:
|
Hello PolaNanElias yes INOX is usually used in such environments. Depends on what size you need: https://support.industry.siemens.com/cs/de/en/view/89332253 https://support.industry.siemens.com/cs/de/en/view/99051118 https://support.industry.siemens.com/cs/de/en/view/109480622 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on