9/6/2023 9:34 AM | |
Joined: 6/7/2023 Last visit: 6/19/2024 Posts: 1 Rating:
|
Greetings, Siemens Community Here, I'm writing about a problem with my HMI Pro CS display. As you can see in the image, the display resolution sometimes changes automatically after HT8 control exchange; the HT8 has a resolution of about 640 x 480, while the HMI display's recommended or standard resolution is 1366 x 768. However, after HT8 control exchange, sometimes the HMI resolution changes automatically when HT8 is disconnected and stays at 640 x 480. AttachmentHMI Pro CS Display Error.pdf (239 Downloads) |
Follow us on