7/22/2008 8:25 AM | |
Posts: 30 Rating: (0) |
hello, i have a hmi tp170b color and i have download with protool, how i can download with wincc flexible in the same panel?? thank u |
7/22/2008 8:57 AM | |
Joined: 4/24/2006 Last visit: 10/16/2024 Posts: 8746 Rating: (1169) |
Hi Skara, You can download a project from WinCC flexible in panel. First of all, you need a project in WinCC flexible. (It even can be a migrated protool project) Then perform an OS update, so the panel gets the image of WinCC flexible, see link: http://support.automation.siemens.com/WW/view/en/19701610 Be sure to transfer 'WinCC flexible' image Then you can transfer WinCC flexible project. And off course you can later use Protool to transfer a project (If you want). You should perform an OS update, but now with 'Protool' image. Hope this helps. Best regards, Wizard |
Follow us on