2/5/2024 10:27 AM | |
Joined: 5/6/2022 Last visit: 6/20/2024 Posts: 422 Rating: (83) |
Hi Swissi1, If I understand you correctly, Comfort panels need to load a Sm@rtServer license up to version V14. Without that license you would not be able to work even if this functionality is enabled. Here you can see the available licenses: "WinCC Sm@rtServer" It is also important that you have enabled the Sm@rtServer option in the project because if it was not enabled, you would need the project to configure it. If this is not what you are asking, I would ask you to specify more what you need! Best regards! |
If this Information really helps, you could use the Rate function |
|
2/6/2024 9:18 PM | |
Joined: 2/23/2022 Last visit: 6/18/2024 Posts: 3 Rating: (0) |
Hi Thank you for the informations Regards |
This contribution was helpful to1 thankful Users |
Follow us on