9/1/2023 12:58 PM | |
Joined: 11/28/2007 Last visit: 6/24/2024 Posts: 20 Rating:
|
Hello, In a project I have a TP1200 Comfort Version 17 with a RFID reader RF1060. On HMI is running HMI Option+ V3.2 with PM-logon enabled. In the console of HMI Option+ are a lot of errors. In the example project project of HMI Options are tags for reading information of for example the status of the reader (statusrfid), but I don't recieve anything. What are we missing? AttachmentError.pdf (437 Downloads) |
9/4/2023 7:31 AM | |
Joined: 5/30/2022 Last visit: 7/17/2024 Posts: 553 Rating:
|
Hi ivh, Reset the Panel to factory settings to resolve the error, I attach information: Updating the operating system of the HMI device Possible cause: Profinet Device Name of the Panel |
If this information really helps, you could use the Rate function. |
|
This contribution was helpful to
1 thankful Users |
9/4/2023 12:59 PM | |
Joined: 11/28/2007 Last visit: 6/24/2024 Posts: 20 Rating:
|
Thank you. After reset everthing works fine. |
Follow us on