9/1/2021 9:30 AM | |
Joined: 9/1/2021 Last visit: 9/8/2022 Posts: 2 Rating: (1) |
Currently I have a similar issue, I have a siemens field pg m6. I had it running fine for more than 1 year no issues. one morning it decided not to restart. I tried to remove the battery and start it with no battery(only the charger). it booted fine. I ordered a new battery and it was the exact same battery (SP306) plugged in, it booted fine, and only lasted 6 months this morning it had a boot error( default boot device missing or boot failed), I tried booting with no battery, my device booted fine, I need assistance as to what my options are regarding the pg and its battery, since its outside siemens warranty now. I this something is wrong with the pg charging circuit/system, since with the battery in it doesn't boot, and it seems to ficker the display slightly, like its shorting somewhere ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/13/2021 14:14:25New subject after splitting |
|
2/7/2022 9:47 PM | |
Joined: 2/28/2017 Last visit: 10/15/2024 Posts: 34 Rating: (1) |
Currently same issue. Will order a new battery. Sometimes you are able to boot with the supposedly bad battery but the screen will flicker as if the battery/charging circuit is trying to do something. And you will also get the "boot device missing". 95% of the time my M6 was connected to the charger.
|
Last edited by: samuelbb at: 02/07/2022 21:49:42 |
|
Follow us on