12/17/2010 1:16 AM | |
Joined: 6/4/2008 Last visit: 6/2/2024 Posts: 1484 Rating: (322) |
Hi, this would probably be better posted under the Simotion Conference. Basically, it sounds like you need to install the Simotion Scout software (The latest version is 6AU1810-1BA41-5XA0)Further information can be found here. Several versions are available, the Standalone version is for users who do not have or need Step 7. You can determine which software packages are missing from your project by clicking the project title, selecting properties and then click on the tab "Required software packages" ) See the attached picture. Be sure you definately need it, as the price is similar to that of Step7. Regards, Graeme |
Follow us on